2.6.2.2
Changing the display form
The form in which disassembled results are displayed can be changed freely by using the toolbar buttons shown below.
|
View
|
Shows the following buttons that change the display form.
|
|
|
|
Displays the offset values of labels. If the address has no labels defined, an offset value from the closest label is displayed.
|
|
|
Displays address values in the form "symbol + offset value" (default).
However, if the address value has a symbol defined, only the symbol is displayed.
|