The Pin Configurator is used to output report files such as a device pin list and a device top view by entering pin assignment information of the microcontroller.
The following sections describe the operation procedures for Pin Configurator.
Launch CS+ from the [Start] menu of Windows.
Create a new project (that defines a kind of project, microcontroller to be used, build tools to be used, etc.) or load an existing project.
Open the Device Pin List panel, where you enter information on the pins of the microcontroller.
Allows you to select items displayed in the device pin list.
Allows you to change the order in which items are displayed in the device pin list.
Allows you to add columns to the device pin list.
Allows you to delete columns from the device pin list.
Open the Device Top View panel, where you can confirm the information entered for the pins.
Allows you to select the shape of the microcontroller displayed in the Device Top View panel.
Allows you to select colors used to distinguish the type of pins (power pins, special pins, used pins, etc.) whose information is displayed in the Device Top View panel.
Allows you to select the type of information that popups when you move the mouse cursor over each pin in the Device Top View panel.
Select the type of information to display in Pin area of the Device Top View panel.
Enter information on the pins of the microcontroller in the Device Pin List panel.
Output report files (files containing configured information using Pin Configurator: device pin list and device top view) to the specified folder.