Everything

Displaying a Special Function Register (SFR)

Displaying SFR

In this section, you observe the value of the register that implements peripheral functions built in the microcontroller. First, let's make the panel float so that it is easier to view.

 

Select [SFR] from the [View] menu.

This opens the SFR panel.

Right-click on the title bar of the SFR panel and check the [Floating].

The SFR panel enters the floating state and it becomes easier to view.