Use this page to display a list of updates hidden in the Select updates page, restore the visibility of the selected updates, and enable that update to be checked and installed again.
![](Updater_Eng-43.gif)
The following items are explained here.
From the CS+ Update Manager window menu area, click [Restore hidden updates]. |
The selected updates become visible, enabling them to be re-checked and installed.
Displays a list of updates that were hidden via the Select updates page.