You can add the currently open project to the menu as a "favorite project" (up to four projects).
From the [Project] menu, select [Favorite Projects] >> [1 - 4 Register to Favorite Project], the path of the currently open project is registered under the [Project] menu >> [Favorite Projects]. The path is also registered in [Favorite project] in the [Open Existing Project] area on the Start panel.
![](ProjectOperation_Eng-24.gif)
![](ProjectOperation_Eng-25.gif)