1.4  Operating Environment
 
Below are the system requirements for this product.
Processor and main memory that can comfortably run the software described in the software environment
Display: Resolution at least 1,024 x 768
Interface: USB 2.0
| 
- | Microsoft .NET Framework 4.6.2 | 
| 
- | Microsoft Visual C++ 2015 Redistributable Update 3 | 
| 
- | Online help: Edge, Internet Explorer, Chrome, or Firefox (The latest version is recommended) | 
| 
(3) | Supported target environments | 
| 
- | Full-spec emulator [RH850] | 
| 
- | E2 emulator [RH850][RX][RL78] | 
| 
- | E2 emulator Lite [RX][RL78] |