Performs processing in response to detection of parity error (ACK error).
[Syntax]
#include “r_cg_macrodriver.h”
static void r_iicmn_callback_master_error ( MD_STATUS flag );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       MD_STATUS flag;  | 
    
       Cause of communication error MD_NACK: Acknowledge not detected  | 
[Argument(s)]
None.
[Return value]
None.