Everything

r_dmacn_callback_transfer_escape_end

Performs processing in response to the escape transfer end interrupt.

Remark         This API function is called as the r_dmac_dmacni_interrupt callback routine, which is generated by escape transfer end.

 

[Syntax]

static void    r_dmacn_callback_transfer_escape_end ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.