Everything

r_iwdt_nmi_interrupt

Performs processing in response to the non-maskable interrupt (WUNI).

Remark         This API function is called to run interrupt processing for the non-maskable interrupt (WUNI), which is generated when the down-counter underflows or refreshing proceeds outside the period where it is permitted.

 

[Syntax]

static void    r_iwdt_nmi_interrupt ( void );

 

[Argument(s)]

None.

 

[Return value]

None.