Changes the operating power control mode of the MCU.
[Syntax]
#include "r_cg_macrodriver.h"
#include "r_cg_lpc.h"
MD_STATUS R_LPC_ChangeOperatingPowerControl ( operating_mode_t mode );
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
operating_mode_t mode; |
Operating power control mode type HIGH_SPEED : High-speed operating mode MIDDLE_SPEED : Middle-speed operating mode LOW_SPEED : Low-speed operating mode |
[Return value]
|
Macro |
Description |
|
MD_OK |
Normal completion |
|
MD_ERROR1 |
Change to the low-speed operating mode ended abnormally. |
|
MD_ERROR2 |
Change to the middle-speed operating mode is ended abnormally. |
|
MD_ARGERROR |
Invalid argument mode specification |