Everything

r_mtu3_tciun_interrupt

Performs processing in response to the underflow interrupt.

Remark         This API function is called to run interrupt processing for the underflow interrupt, which is generated in response to an underflow of the timer counter (TCNT).

 

[Syntax]

static void    r_mtu3_tciun_interrupt ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.