Performs user-defined initialization relating to the port output enable 3.
Remark This API function is called as the R_POE3_Create callback routine.
[Syntax]
void R_POE3_Create_UserInit ( void );
[Argument(s)]
None.
[Return value]
None.
Performs user-defined initialization relating to the port output enable 3.
Remark This API function is called as the R_POE3_Create callback routine.
[Syntax]
void R_POE3_Create_UserInit ( void );
[Argument(s)]
None.
[Return value]
None.