Sets the condition for the alarm interrupt (ALM) and allows detection of ALM (binary count mode).
[Syntax]
void R_RTC_Set_BinaryAlarm ( uint32_t alarm_enable, uint32_t alarm_val );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       uint32_t alarm_enable;  | 
    
       Comparison flag 0x0 : Comparison does not proceed 0x1 : Comparison proceeds  | 
| 
       I  | 
    
       uint32_t alarm_val;  | 
    
       The value of the binary counter  | 
[Return value]
None.