Everything

R_SCIn_SPI_Master_Send_Receive

Starts SCI master transmission/reception (simple SPI mode).

Remark 1.      This API function repeats SCI master transmission in byte units the number of times specified by the argument tx_num from the buffer at the location specified by the argument tx_buf.

Remark 2.      This API function repeats SCI master reception in byte units the number of times specified by the argument rx_num and the received data are stored in the buffer at the location specified by the argument rx_buf.

Remark 3.      When performing a SCI master transmission/reception, R_SCIn_Start must be called before this API function is called.

 

[Syntax]

#include       "r_cg_macrodriver.h"

MD_STATUS   R_SCIn_SPI_Master_Send_Receive ( uint8_t * const tx_buf, uint16_t tx_num,

uint8_t * const rx_buf, uint16_t rx_num );

Remark         n is the channel number.

 

[Argument(s)]

I/O

Argument

Description

I

uint8_t * const tx_buf;

Pointer to a buffer storing the transmission data

I

uint16_t tx_num;

Total amount of data to send

O

uint8_t * const rx_buf;

Pointer to a buffer to store the reception data

I

uint16_t rx_num;

Total amount of data to receive

 

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ARGERROR

Invalid argument tx_num specification