Everything

vrst_mpf

Outline
Reset fixed-sized memory pool.
C format
 ER      vrst_mpf (ID mpfid);
Parameter(s)
I/O
Parameter
Description
I
 ID      mpfid;
ID number of the fixed-sized memory pool.

Explanation
This service call reset the fixed-sized memory pool specified by parameter mpfid.
The tasks to wait to get memory block from the target fixed-sized memory pool are released from the WAITING state, and EV_RST is returned as a return value for the tasks.
Note 1 All fixed-sized memory blocks that had already been acquired are returned to the target fixed-sized memory pool. Therefore, do not access those fixed-sized memory blocks after issuing this service call.
Note 2 This service call is the function outside mITRON4.0 specification.
Return value
Macro
Value
Description
E_OK
0
Normal completion.
E_ID
-18
Invalid ID number.
- mpfid < 0
- mpfid > VTMAX_MPF
E_CTX
-25
Context error.
- This service call was issued from a non-task.
- This service call was issued in the CPU locked state.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
E_MACV
-26
Memory access violation.
- Stack pointer points out of user stack for invoking task.
E_NOEXS
-42
Non-existent object.
- The fixed-sized memory pool specified by mpfid does not exist.