-
sta_tsk
ista_tsk
-
Activate task (does not queue an activation request).
ER sta_tsk ( ID tskid, VP_INT stacd );
ER ista_tsk ( ID tskid, VP_INT stacd );
|
MOVW BC, #stacd_lo
MOVW DE, #stacd_hi
MOV A, #tskid
CALL !!_sta_tsk
MOVW BC, #stacd_lo
MOVW DE, #stacd_hi
MOV A, #tskid
CALL !!_ista_tsk
|
|
|
|
|
|
|
ID tskid;
|
ID number of the task to be activated.
|
|
|
VP_INT stacd;
|
|
These service calls move a task specified by parameter
tskid from the DORMANT state to the READY state.
As a result, the target task is queued at the end on the ready queue corresponding to the initial priority and becomes subject to scheduling by the RI78V4.
Note 1 This service call does not perform queuing of activation requests. If the target task is in a state other than the DORMANT state, the counter manipulation processing is therefore not performed but "E_OBJ" is returned.
Note 2 A start code "
stacd" is passed to the task activated by issuing this service call.
|
|
|
|
|
|
|
|
|
|
|
Object state error (specified task is not in the DORMANT state).
|