Initializes a 2-byte area with the specified value, right-shifted one bit.
[Syntax]
|
Symbol field
|
Mnemonic field
|
Operand field
|
Comment field
|
[label:]
|
.dshw
|
expression[, ... ]
|
[; comment]
|
[Function]
- | Initializes a 2-byte area with the specified value, right-shifted one bit. |
[Description]
- | The value is allocated as 2-byte data, as the value of the expression right-shifted 1 bit. |
- | If the relocation attribute of the section is "BSS", then an error is output because the .dshw directive cannot be described. |
- | It is possible to code an absolute expression in the operand expression. |
- | The value of the expression, right-shifted one bit, must be in the range 0x0 to 0xFFF. In other cases, the data from the lower two bytes will be allocated. |
- | Any number of expressions may be specified on a single line, by separating them with commas. |
- | It is not possible to code string constants in the operand. |