Everything
Everything
top
RX Debug Tool
FUNCTIONS
Configuration of Operating Environment of the Debug Tool
2.3
Configuration of Operating Environment of the Debug Tool
This section describes the configuration of the operating environment for each debug tool.
To the latest version of this page
Differences Information
Previous Topic
[Simulator]
Next Topic
Select the debug tool to use
Table of Contents
Overview
Preparation before Debugging
Configuration of Operating Environment of the Debug Tool
Select the debug tool to use
[E1]
[E20]
[EZ Emulator]
[Simulator]
Connect to/Disconnect from the Debug Tool
Download and Upload
Displaying and Changing Programs
Usage of PIC/PID Function
Setting Overlay Sections
Execute Programs
Stop Programs (Break)
Displaying and Changing Memory, Registers, and Variables
Display Function Call Information from the Stack
Collecting an Execution History
Measuring the Execution Time
Measure Coverage [Simulator] [E20 [RX71M, RX66x, RX65x, RX64M, RX66T, RX671, RX72T, RX72M, and RX72N Groups]]
Set an Action into Programs
Event Management
Setting Up the Hook Process
Measuring Current Consumption [E2]
Using the Debug Console
About Input Value
Differences between the Microcontroller and the Emulator
Other Notes on Usage [E1] [E20] [EZ Emulator]