Everything
2.13.3.2 Combining multiple events [E1] [E20] [EZ Emulator]

If there are two or more events set for the trace start event, collection of trace data can be made to start when the trace start event satisfies the following combination conditions.

Also, if there are two or more events set for the trace end event, collection of trace data is finished when the condition for any one of trace end events is met.

Table 2.13

Combination Conditions for the Trace Start Event

Combination condition

Description

OR

Collection of trace data begins when any one of the trace start events set occurs (i.e., its designated condition is met).

AND

Collection of trace data begins when all of the trace start events set occur, irrespective of time base.

Sequential

Collection of trace data begins when the trace start events set occur in a specified order.

Also, an event, but only one, of trace start events can be registered as a reset event (R event). When a registered event occurs, the other trace start events that have had occurred up to that point of time are all cleared.

To edit a set trace event, choose [Event] from the [View] menu, select the trace event on the Events panel that is opened, and then click [Edit Condition ...] on the context menu.

Do your editing in a dialog box that is opened by this operation.

For details on how to edit in a dialog box, see “2.17.4.3 Editing combination conditions of events [E1] [E20] [EZ Emulator]”.

Caution

Also see Cautions of "(1) Editing the combination condition" for details on combination conditions.