Everything

debugger.ProcesserElementName


This property sets or refers to the PE of multiple cores with the name.

[Specification format]

debugger.ProcessorElementName = name

[Setting(s)]

Setting

Description

name

Set the PE name as a string.

[Reference]

Current set value

[Detailed description]

-

This property sets or refers to the PE of the multi-core.

-

The specifiable strings can be obtained by calling debugger.GetProcesserElementNames.

Caution

When the PE is set, it must be connected to the debugging tool.

[Example of use]

>>>print debugger.ProcessorElementName
CPU1
>>>debugger.ProcessorElementName = 'CPU2'
>>>print debugger.ProcessorElementName
CPU2
>>>