| 
 Add Folder and File dialog box 
 | 
This dialog box is used to add existing files and folder hierarchies to the project.
The folder is added as a category.
Figure A.10  | Add Folder and File Dialog Box  | 
 
 
The following items are explained here.
[How to open]
[Description of each area]
Select the type of the file to be added to the project.
You can select multiple file types by left clicking while holding down the [Ctrl] or [Shift] key.
If nothing is selected, it is assumed that all types are selected.
(2)  | [Subfolder level to search] area  | 
 
Directly enter the number of levels of the subfolder to be added to the project.
"1" is displayed by default.
Remark  | Up to 10 (decimal number) can be specified. 
When the input violates any restriction, the following messages will be shown in the tooltip.  | 
 
| 
 | 
 | 
| 
 
Fewer than 0 or more than 10 values cannot be specified. 
 | 
 
More than 10 subfolder levels have been specified. 
 | 
| 
 
Specify in decimal. 
 | 
 
A number in other than decimal or a string has been specified. 
 | 
 
Caution  | The name of a network path cannot be used. Assign the name of a path on a drive.  | 
 
[Function buttons]
| 
 | 
 | 
| 
 
OK 
 | 
 
Adds the folder that was dragged and dropped and the files in that folder to the project.  And then closes this dialog box. 
 | 
| 
 
Cancel 
 | 
 
Does not add the folder and files, and then closes this dialog box. 
 | 
| 
 
Help 
 | 
 
Displays the help of this dialog box. 
 |