Everything
2.10 Register Watch-Expressions

You can register variables on the Variable List panel as watch-expressions in the Watch panel (Watch1).

To do this, drag and drop the row of the target variable (multiple selections possible) directly onto the Watch panel (Watch1).

Cautions 1.

This operation is disabled while disconnecting from the debug tool.

Cautions 2.

This operation is disabled for the [*Total*] row.

Remark

The name of the watch-expression registered in the Watch panel differs depending on the type of the target variable, as follows:

-

Global variable: "variable name"

-

Static variable inside a file: "file name#variable name"

-

Static variable inside a function: "file name#function name#variable name"

-

Class variable: "class name::variable name"