| R_ADCn_ScanGroupm_GetResult | 
Reads the results of ADC scan group conversion.
[Syntax]
| void    R_ADCn_ScanGroupm_GetResult ( uint16_t * buffer ); | 
| 
Remark | n is the unit number, m is the scan group number. | 
[Argument(s)]
|  |  |  | 
|  | uint16_t  * buffer; | 
Pointer to area in which to store the results of A/D conversion | 
[Return value]
None.