Reads the results of DFE processing calculation.
[Syntax]
| void    R_DFE_Channelm_GetResult ( int32_t * buffer ); | 
| 
Remark | m is the channel number. | 
[Argument(s)]
|  |  |  | 
|  | int32_t * buffer; | 
Pointer to area in which to store the results of DFE processing calculation | 
[Return value]
None.