Sets the counter value of the real-time clock.(in the case of the binary mode setting)
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_rtc.h”
MD_STATUS R_RTC_Set_BinaryCounterValue ( uint32_t counter_write_val );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       uint32_t counter_write_val;  | 
    
       Counter value  | 
[Return value]
| 
       Macro  | 
    
       Description  | 
| 
       MD_OK  | 
    
       Normal completion  | 
| 
       MD_BUSY1  | 
    
       Executing count process (before change to setting)  | 
Remark If MD_BUSY1 is returned, it may be because the counter operation start wait time is too short, so make the value of the RTC_WAITTIME macro defined in the header file "r_cg_rtc.h" larger.