Starts UARTMG data transmission.
Remarks 1. This API function repeats the byte-level UART transmission from the buffer specified in argument tx_buf the number of times specified in argument tx_num.
Remarks 2. When performing a UART transmission, R_UARTMGn_Start must be called before this API function is called.
[Syntax]
#include “r_cg_macrodriver.h”
MD_STATUS R_UARTMGn_Send ( uint8_t * const tx_buf, uint16_t tx_num );
Remark n is the channel number.
[Argument(s)]
| I/O | Argument | Description | 
| I | uint8_t * const tx_buf; | Pointer to a buffer storing the transmission data | 
| I | uint16_t tx_num; | Total amount of data to send | 
[Return value]
| Macro | Description | 
| MD_OK | Normal completion | 
| MD_ARGERROR | Invalid argument specification |