Usage example (Pulse output mode)
Perform toggle operation at fixed intervals and output a suquare wave with a duty factor of 50%.
[Waveform example]

[GUI setting example]
| 
       Timer  | 
    
       Used  | |||
| 
       TMRJ0  | 
    
       Used  | |||
| 
       Functions  | 
    
       Pulse output mode  | |||
| 
       Count source setting  | 
    
       Auto  | |||
| 
       Timer value  | 
    
       100μs (Actual value:100)  | |||
| 
       Output (TRIJO0)  | 
    
       Starts as “H”  | |||
| 
       Enable output(TRJO0)  | 
    
       Unused  | |||
| 
       When the counter underflows, generate an interrupt (INTTRJ0)  | 
    
       Used  | |||
| 
       Priority  | 
    
       Low  | |||
[API setting example]
r_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start TMRJ0 counter */
R_TMR_RJ0_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}