Performs processing in response to the input capture/compare match interrupt.
[Syntax]
static void r_gpt_gtcimn_interrupt ( void );
Remark m is the timer general register number, n is the channel number.
[Argument(s)]
None.
[Return value]