Everything

R_LPC_ChangeOperatingPowerControl

Changes the operating power control mode of the MCU.

 

[Syntax]

#include       "r_cg_macrodriver.h"

#include       "r_cg_lpc.h"

MD_STATUS   R_LPC_ChangeOperatingPowerControl ( operating_mode_t mode );

 

[Argument(s)]

I/O

Argument

Description

I

operating_mode_t mode;

Operating power control mode type

HIGH_SPEED                     : High-speed operating mode

MIDDLE_SPEED                : Middle-speed operating mode

LOW_SPEED                      : Low-speed operating mode

 

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ERROR1

Change to the low-speed operating mode ended abnormally.

MD_ERROR2

Change to the middle-speed operating mode is ended abnormally.

MD_ARGERROR

Invalid argument mode specification