Performs processing in response to the output enable interrupt.
Remark This API function is called to run interrupt processing for the output enable interrupt, which is generated when a related pin becomes high-impedance or the output short flag 1 is set.
[Syntax]
static void r_poe3_oein_interrupt ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.