Sets the calendar and time values.
[Syntax]
#include "r_cg_rtc.h"
void R_RTC_Set_CalendarCounterValue ( rtc_calendarcounter_value_t counter_write_val );
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
rtc_calendarcounter_value_t counter_write_val; |
Calendar and time values (year, month, date, day-of-week, time, minute, and second) |
Remark The configuration of the calendar and time values rtc_calendarcounter_value_t is shown below.
|
typedef struct { uint8_t rseccnt; /* second */ uint8_t rmincnt; /* Minute */ uint8_t rhrcnt; /* Time */ uint8_t rdaycnt; /* Date */ uint8_t rwkcnt; /* Day-of-week (0: Sunday, 6: Saturday) */ uint8_t rmoncnt; /* Month */ uint16_t ryrcnt; /* Year */ } rtc_calendarcounter_value_t; |
[Return value]
None.