Sets compare level.
[Syntax]
void R_S12ADn_Set_CompareValue ( uint16_t reg_value0, uint16_t reg_value1);
Remark n is the unit number.
[Argument(s)]
I/O |
Argument |
Description |
I |
uint16_t reg_value0; |
Register value set to the compare revel register 0 |
I |
uint16_t reg_value1; |
Register value set to the compare revel register 1 |
[Return value]
None.