Everything

r_scifan_teif_interrupt

Performs processing in response to the transmit-end interrupts.

Remark         This API function is called to run the interrupt processing for the transmit-end interrupt.

 

[Syntax]

static void    r_scifan_teif_interrupt ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.