Starts SCI slave transmission/reception (simple SPI mode).
Remark 1. This API function repeats SCI slave transmission in byte units the number of times specified by the argument tx_num from the buffer at the location specified by the argument tx_buf.
Remark 2. This API function repeats SCI slave reception in byte units the number of times specified by the argument rx_num and the received data are stored in the buffer at the location specified by the argument rx_buf.
Remark 3. When performing a SCI slave transmission/reception, R_SCIn_Start must be called before this API function is called.
[Syntax]
#include "r_cg_macrodriver.h"
MD_STATUS R_SCIn_SPI_Slave_Send_Receive ( uint8_t * const tx_buf, uint16_t tx_num,
uint8_t * const rx_buf, uint16_t rx_num );
Remark n is the channel number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       uint8_t * const tx_buf;  | 
    
       Pointer to a buffer storing the transmission data  | 
| 
       I  | 
    
       uint16_t tx_num;  | 
    
       Total amount of data to send  | 
| 
       O  | 
    
       uint8_t * const rx_buf;  | 
    
       Pointer to a buffer to store the reception data  | 
| 
       I  | 
    
       uint16_t rx_num;  | 
    
       Total amount of data to receive  | 
[Return value]
| 
       Macro  | 
    
       Description  | 
| 
       MD_OK  | 
    
       Normal completion  | 
| 
       MD_ARGERROR  | 
    
       Invalid argument tx_num specification  |