Performs user-defined initialization relating to the 8-bit timer.
Remark This API function is called as the R_TMR_Create callback routine.
[Syntax]
void R_TMR_Create_UserInit ( void );
[Argument(s)]
None.
[Return value]
None.
Performs user-defined initialization relating to the 8-bit timer.
Remark This API function is called as the R_TMR_Create callback routine.
[Syntax]
void R_TMR_Create_UserInit ( void );
[Argument(s)]
None.
[Return value]
None.