Everything
2.3.2 Icon indicating incorrect entry

When performing code generation, if you enter an invalid string in the Peripheral Functions panel, or a required input is missing, then a icon displays next to the incorrect input, and the text is displayed in red to warn that there is a problem with the input.

Figure 2.2

Icon Indicating Incorrect Entry

 

Remark

If the mouse cursor is moved over the icon, information regarding the string that should be entered (tips for correcting the entry) popups.