Output the source code (device driver program) by pressing the
button on the Peripheral Functions panel.
The destination folder for the source code is specified by clicking [Code Generator Setting] tab >> [Generate File Mode] >> [Output folder] in the Property panel.
![](r20ut3104ej0110_cscgpf-11.gif)
In order to both output source files and add them to the project (display the corresponding source file names in the Project Tree panel) when you click the |
![](r20ut3104ej0110_cscgpf-13.gif)