Everything

tsnd_dtq

Outline
Send to data queue (with timeout).
C format
 ER      tsnd_dtq ( ID dtqid, VP_INT data, TMO tmout );

Assembly format
 MOVW    DE, !LOWW(_data+0x00002)
 MOVW    BC, !LOWW(_data)
 MOVW    AX, #tmout_hi
 PUSH    AX
 MOVW    AX, #tmout_lo
 PUSH    AX
 MOV     A,  #dtqid
 CALL    !!_tsnd_dtq

Parameter(s)
I/O
Parameter
Description
I
 ID      dtqid;
ID number of the data queue to which the data element is sent.
I
 VP_INT  data;
Data element to be sent to the data queue.
I
 TMO     tmout;
Specified timeout (in tick).
TMO_FEVR: Waiting forever.
TMO_POL: Polling.
Value: Specified timeout.

Explanation
This service call writes data specified by parameter data to the data queue area of the data queue specified by parameter dtqid.
If there is no available space for writing data in the data queue area of the target data queue when this service call is issued, the service call does not write data but queues the invoking task to the transmission wait queue of the target data queue and moves it from the RUNNING state to the WAITING state with time (data transmission wait state).
The sending WAITING state for a data queue is cancelled in the following cases, and then moved to the READY state.
Sending WAITING State for a Data Queue Cancel Operation
Return Value
An available space was secured in the data queue area of the target data queue as a result of issuing rcv_dtq.
E_OK
An available space was secured in the data queue area of the target data queue as a result of issuing prcv_dtq.
E_OK
An available space was secured in the data queue area of the target data queue as a result of issuing trcv_dtq.
E_OK
Forced release from waiting (accept rel_wai while waiting).
E_RLWAI
Forced release from waiting (accept irel_wai while waiting).
E_RLWAI
Polling failure or timeout.
E_TMOUT

If a task has been queued to the reception wait queue of the target data queue when this service call is issued, this service call does not write data but transfers the data to the task. As a result, the task is unlinked from the reception wait queue and moves from the WAITING state (data reception wait state) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
Note 1 Data is written to the data queue area of the target data queue in the order of the data transmission request.
Note 2 Invoking tasks are queued to the transmission wait queue of the target data queue in the order defined during configuration (FIFO order).
Note 3 TMO_FEVR is specified for wait time tmout, processing equivalent to snd_dtq will be executed. When TMO_POL is specified, processing equivalent to psnd_dtq /ipsnd_dtq will be executed.
Return value
Macro
Value
Description
E_OK
0
Normal completion.
E_RLWAI
-49
Forced release from the WAITING state.
- Accept rel_wai/irel_wai while waiting.
E_TMOUT
-50
Timeout.
- Polling failure or timeout.