|
-reent [V2.03.00 or later]
|
< Library Generator Options / Library Options >
[Format]
[Description]
- | This option creates reentrant libraries. |
- | Note that the rand, srand and EC++ library functions are not reentrant libraries. |
[Remarks]
- | This option is available in V2.03 and later versions of this compiler. |
- | When reentrant libraries are linked, use #define to define the macro name of _REENTRANT before including standard include files in the program or use the -define option to define _REENTRANT at compilation. |