Startup routine that The Renesas integrated development environment (IDE) for RX Family supplies is as follows:
Table 8.1  | List of Programs Created in Integrated Development Environment  | 
 
| 
 | 
 | 
 | 
| 
 
(a) 
 | 
 
resetprg.c 
 | 
 
Initial setting routine (reset vector function) 
 | 
| 
 
(b) 
 | 
 
intprg.c 
 | 
 
Vector function definitions 
 | 
| 
 
(c) 
 | 
 
vecttbl.c 
 | 
 
Fixed vector table*1 
 | 
| 
 
(d) 
 | 
 
dbsct.c 
 | 
 
Section initialization processing (table) 
 | 
| 
 
(e) 
 | 
 
lowsrc.c 
 | 
 
Low-level interface routine (C language part) 
 | 
| 
 
(f) 
 | 
 
lowlvl.src 
 | 
 
Low-level interface routine (assembly language part) 
 | 
| 
 
(g) 
 | 
 
sbrk.c 
 | 
 
Low-level interface routine (sbrk function) 
 | 
| 
 
(h) 
 | 
 
typedefine.h 
 | 
 
Type definition header 
 | 
| 
 
(i) 
 | 
 
vect.h 
 | 
 
Vector function header 
 | 
| 
 
(j) 
 | 
 
stacksct.h 
 | 
 
Stack size settings 
 | 
| 
 
(k) 
 | 
 
lowsrc.h 
 | 
 
Low-level interface routine (C language header) 
 | 
| 
 
(l) 
 | 
 
sbrk.h 
 | 
 
Low-level interface routine (sbrk function header) 
 | 
 
Notes 1.  | This is for the RXv1 instruction-set architecture. 
For an RX instruction-set architecture other than the RXv1 instruction-set architecture, this becomes the "exception vector table".  |