The I/O register values can be edited.
Select the value of the I/O register to edit in the [Value] area, then click on it again to switch the value to edit mode (press the [Esc] key to cancel the edit mode).
To write the edited value to the target memory, directly enter the value from the keyboard then press the [Enter] key.
If a number with fewer digits than the size of the I/O register is entered, the higher-order digits will be padded with zeroes. |
If a number with more digits than the size of the I/O register is entered, the higher-order digits will be masked. |
When the numeric "0x41" is written to the I/O register "OSTMnXX" |