Everything
Everything
top
RX Debug Tool
FUNCTIONS
2.
FUNCTIONS
This chapter describes the debugging process using CS+ as well as main debugging functions.
To the latest version of this page
Differences Information
Previous Topic
Features
Next Topic
Overview
Table of Contents
GENERAL
FUNCTIONS
Overview
Preparation before Debugging
Configuration of Operating Environment of the Debug Tool
Connect to/Disconnect from the Debug Tool
Download and Upload
Displaying and Changing Programs
Usage of PIC/PID Function
Setting Overlay Sections
Execute Programs
Stop Programs (Break)
Displaying and Changing Memory, Registers, and Variables
Display Function Call Information from the Stack
Collecting an Execution History
Measuring the Execution Time
Measure Coverage [Simulator] [E20 [RX71M, RX66x, RX65x, RX64M, RX66T, RX671, RX72T, RX72M, and RX72N Groups]]
Set an Action into Programs
Event Management
Setting Up the Hook Process
Measuring Current Consumption [E2]
Using the Debug Console
About Input Value
Saving and Restoring the States of Debug Tools
Differences between the Microcontroller and the Emulator
Other Notes on Usage [E1] [E20]
WINDOW REFERENCE
I/O FUNCTIONS
COPYRIGHT