Everything

Output panel


This panel displays operation logs for various components (design tool, build tool, etc.) provided by CS+.

The messages are classified by the message origination tool and displayed on the individual tabs.

Remark

The Message area can be zoomed in and out by in the tool bar, or by operating the mouse wheel while holding down the [Ctrl] key.

Figure A.11

Output Panel

 

The following items are explained here.

[How to open]

-

From the [View] menu, select [Output].

[Description of each area]

(1)

Message area

The output messages of each tool are displayed.

Note that the character colors/background colors of the message differ with the type of output message (and depend on the settings in the [General - Font and Color] category in the Option dialog box).

(2)

Tab selection area

Select the tab that indicates the origin of message.

The following tabs are available for the Code Generator.

All Messages

Displays operation logs for all components (design tool, build tool, etc.) provided by CS+ in order of output.

Code Generator

Display only operation logs for the Code Generator out of those for various components (design tool, build tool, etc.) provided by CS+.

Caution

Even if a new message is output on a deselected tab, tab selection will not automatically switch. In this case, " * " mark will be added in front of the tab name, indicating that a new message has been output.

[Context menu]

Copy

Sends the character string or lines selected with range selection to the clipboard.

Select All

Selects all the messages displayed on the Message area.

Clear

Deletes all the messages displayed on the Message area.

Tag Jump

Jumps to the caret line in the editor indicated by the message (file, line, and column).

Open Help for Message

Displays help for the message on the current caret location.

This only applies to warning messages and error messages.