Everything

3.3 Abort Errors

Table 3-3. Abort Errors
[Message]
Option (xxx) is not specified.
[Action by User]
Make sure whether the configuration file input to an option is specified.
[Message]
Cannot open device file.
[Action by User]
Make sure that the device file exists.
[Message]
File name (xxx) is duplicated.
[Message]
Option (xxx) needs parameters.
[Action by User]
Check the option.
[Message]
[RI850V4 V1.xx.xx] [RI850V4 V2.xx.xx]
The parameters (xxx) is illegal.
[Action by User]
[RI850V4 V1.xx.xx] [RI850V4 V2.xx.xx]
Check the parameter.
[Message]
[RI850MP]
Illegal parameters (xxx).
[Action by User]
[RI850MP]
Check the parameter.
[Message]
The option (xxx) is Illegal.
[Action by User]
Check the option.
[Message]
Illegal format is in command file.
[Action by User]
Check the contents of a command file.
[Message]
Path or file name is too long (xxx).
[Message]
File (xxx) is not a supported file to convert.
[Message]
A described device (xxx) is not supported.
[Message]
The size of the command (xxx) file is too big.
[Message]
Cannot open command file.
[Explanation]
The specified command file could not be opened. Otherwise, the specified command file name is not valid.
[Action by User]
Check whether the specified command file exists or whether the command file name is correct.
[Message]
[RI78V4 V1.xx.xx]
Usage:CF78V4 [@command file] [-i <SIT file> | -ni] [-dc <C header file> | -ndc] [-da <ASM header file> | -nda] [-V] [-help] <CF file>
[RI78V4 V2.xx.xx]
Usage: CF78V4 [@command file] [-cpu <Name>] [-devpath=<Path>] [-i <SIT file> | -ni] [-dc <C header file> | -ndc] [-da <ASM header file> | -nda] [-V] [-help] <CF file>
[Explanation]
Because the specified activation option is not correct, CF78V4 could not be executed.
[Action by User]
Check the activation option.
[Message]
Option (xxx) is multiple defined.
[Action by User]
Check the contents of a command file.
[Message]
Output file names are the same (xxx).
[Explanation]
The output files (system information table file, system information header file (for C language) or system information header file (for assembly languages)) are specified with the same file name "xxx".
[Action by User]
Check if the file names specified with the -i, -dc, and -da options are the same.
[Message]
It is necessary to specify the device file in the case of outputing entry file.
[Action by User]
Check the specified the output option of the entry file or the device file.
[Message]
It failed to convert file (xxx).
[Message]
Syntax too complecated.
[Action by User]
Check the description of the system configuration file.
[Message]
Unknown device file format.
[Action by User]
Check the device file.
[Message]
File read error (xxx).
[Explanation]
File (xxx) cannot be read.
[Action by User]
Check if the specified file exists. Alternatively, check whether the file name is correct or whether the file name is specified with the valid number of characters.
[Message]
File write error (xxx).
[Explanation]
File (xxx) could not be opened.
[Action by User]
Check whether the file is write-enabled or whether the disk is full. Alternatively, check if the number of characters for the specified file name or output file name converted to an absolute path is valid.
[Message]
[RI850V4 V1.xx.xx] [RI850V4 V2.xx.xx]
Cannot execute Preprocessor.
[Action by User]
[RI850V4 V1.xx.xx] [RI850V4 V2.xx.xx]
Check the pass of a preprocessor and the option.
[Message]
[RI850MP]
Cannot execute Preprocessor (xxx).
[Message]
Too many errors.
[Message]
File name has already existed (xxx).
[Message]
Not enough memory.
[Explanation]
The available memory is insufficient.
[Action by User]
The available memory is insufficient.
The available memory is insufficient to analyze the activation option/command file or to analyze the system configuration file. Increase the memory capacity available for CF78V4 by quitting any applications that are not in use.
[Message]
[RI850V4 V2.xx.xx]
PEID(xxx) is not defined in the device file.
[Explanation]
[RI850V4 V2.xx.xx]
The specified PEID(xxx) is not defined in the device file.
[Action by User]
[RI850V4 V2.xx.xx]
Check the PE number as specified "-peid" option.
[Message]
[RI850V4 V2.xx.xx]
Cannot read xxx in the device file.
[Explanation]
[RI850V4 V2.xx.xx]
Cannot read the information "xxx" from the device file.
[Action by User]
[RI850V4 V2.xx.xx]
Renews the latest device file or reconsiders the specified option.
[Message]
[RI850V4 V1.xx.xx] [RI850V4 V2.xx.xx]
CF850V4 internal error (xxx).
[Action by User]
[RI850V4 V1.xx.xx] [RI850V4 V2.xx.xx]
Please contact your vendor or your Renesas Electronics overseas representative.
[Message]
[RI850MP]
CF850MP internal error (xxx).
[Action by User]
[RI850MP]
Please contact your vendor or your Renesas Electronics overseas representative.