Method of Real-time Sampling

This section describes the real-time sampling method.
This method uses variable values acquired by the RAM monitoring function as the source data for the graph display. A conceptual diagram is shown below.

By default, the sampling-time interval is 500 ms. This interval can be set to as low as 100 ms. Let us try this now. Reduce the sampling interval by following the steps below.
|
In the debugging tool's properties, set the display update interval [ms] to "100", and run the program as before. Next, Stop the program. |




|
A line chart with a sampling interval of 100 ms appears in Analysis Chart . |
You can see that the plot interval is 100 ms, showing more fine-grained data than last time.