Overview of Analysis Feature Demo Program

This section describes the program used to demonstrate the analysis features, and provides an overview of the debug tool.
- Overview of Demo Program
The program we will be using to demonstrate the analysis features is shown below. This is a simple program consisting primarily of a main-routine process and two interrupt processes.

- Overview of the Debugging Tool
A simulator is used as a debugging tool. The simulator is able to simulate the behavior of a microcontroller virtually on the host machine.