Appendix Contents of Information List Panel

Below chart describes contents of Function List Panel. For the details, refer to help.
"Static" information is described after build. "Dynamic" information is described after connecting the debug tool.
|
Description |
Overview |
Static/Dynamic |
|
Function name |
Function name defined/referenced in C source |
Static |
|
File name |
File name of C source where the function is defined |
Static |
|
File Path |
Absolute path of the C source file where the function is defined. |
Static |
|
Import |
Source of the function information |
Static |
|
Attribute |
Function's symbol attributes/symbol-modifier attributes |
Static |
|
Return Type |
Return type of the function |
Static |
|
Arguments count |
Argument value of the function |
Static |
|
Arguments |
Argument type/formal argument name of the function |
Static |
|
Code Size |
Function's code size |
Static |
|
Stack Size |
Function's stack size |
Static |
|
Start Address |
Function's start address |
Static |
|
End Address |
End address of the function |
Static |
|
Reference Count |
Number of times the function is referenced in the program |
Static |
|
Execution Count |
Number of times the function was executed |
Dynamic |
|
Execution Time |
Execution time of the function, Proportion of total, etc.. |
Dynamic |
|
Code Coverage |
Code coverage ratio of the function |
Dynamic |
|
Total |
Total of above item in the target file |
- |