When running a build that targets a specific debug-dedicated project (main project or subproject), you must set that project as the "active project".
The active project is the project subjected to debugging. |
To set the active project, select the Project node to be set as the active project on the project tree and select [Set selected subproject as Active Project] from the context menu.
![](ProjectOperation_Eng-591.gif)
When a project is set as the active project, that Project node is underlined as follows.
![](ProjectOperation_Eng-592.gif)
When you remove a subproject that set as the active project from a project, the main project will be the active project. |