A batch build is a function that builds, rebuilds and cleans are run in batch with the build modes that the project (main project and subproject) has.
Select [Batch Build] from the [Build] menu. The Batch Build dialog box will open.
![](ProjectOperation_Eng-602.gif)
In the dialog box, the list of the combinations of the names of the main project and subprojects in the currently opened project and their build modes and macro definitions ([Defined macros] is invalid when the target project is a debug-dedicated project) is displayed.
Select the check boxes for the combinations of the main project and subprojects and build modes that you wish to run a batch build, and then click the [Build], [Rebuild], or [Clean] button.
Build: "E.5.1 Run a build" |
Rebuild: "E.5.2 Run a rebuild" |
Clean: "E.5.3 Run a clean" |
The batch build order follows the project build order, the order of the subprojects, main project. |
If there are files being edited with the Editor panel when running a batch build, then all these files are saved. |
If a project other than a debug-dedicated project is included in your projects, then builds/rebuilds/cleans will be run for that project using the build tool provided by CS+ (see the "2.8 Run a Build"). |