This dialog box displays all the figure objects created in the I/O Panel window as well as the pin connection status of part objects.
The pin connection settings for each object can be changed in the property dialog box, which can be opened by double-clicking the relevant object listed in this dialog box, or selecting the relevant object listed in this dialog box and then selecting the [View] menu >> [Properties...].
Figure A.96 | Parts List Dialog Box |
This section describes the following.
[How to open]
- | With the I/O Panel window in focus, select [Parts List...] form the [View] menu. |
[Description of each area]
(1) | Pin connection status display area |
|
Label
|
Displays the label (name) attached to the object. Nothing is displayed for objects that do not have a label.
|
|
Parts
|
Displays the part category.
|
|
rectangle
|
Straight line, rectangle, ellipse, rounded rectangle, fan shape
|
|
polygon
|
Polygon
|
|
text
|
Text
|
|
bitmap
|
Bitmap
|
|
button
|
Push button, pull button, group button
|
|
analog button
|
Analog button
|
|
key
|
Key matrix
|
|
level gauge
|
Level gauge
|
|
led
|
LED
|
|
7segment led
|
7-segment LED
|
|
14segment led
|
14-segment LED
|
|
matrix led
|
Matrix LED
|
|
buzzer
|
Buzzer
|
|
groups
|
Grouped part
|
|
Pin Name
|
Displays the pins connected to parts.
"-" is displayed for parts that are connected to multiple pins, and a blank is displayed for parts that are unconnected.
|
|
Active Level
|
Displays the active value set for the part.
"-" is displayed for parts that are connected to multiple pins, and a blank is displayed for parts that are unconnected.
|
[Function buttons]
|
|
|
|
Close
|
Closes the this dialog box.
|